Pulse Building

Wobbulation Types

PRI Wobbulation type sets the wobbulation type that is applied to the PRI pattern. The wobbulation pattern is calculated assuming an ideal signal from the PRI pattern. For a positive deviation, the wobbulation pattern always starts at 0 and increases. For a negative deviation, the wobbulation pattern always starts at 0 and decreases.

Available PRI wobbulation types are:

A 50 Hz sawtooth wobbulation of 5 us applied to a 100 us PRI.